AXIS#.VL.LMJR
Description
This parameter is used in the internal calculation of the current loop acceleration feed forward gain value.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
NA |
|
Range |
0 to 100.0 |
|
Default Value |
0 |
|
Data Type |
Float |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.VL.LMJR | 0x5011 | 0xB | UDINT | 1000:1 | - | RW | False |
| AXIS2.VL.LMJR | 0x5111 | 0xB | UDINT | 1000:1 | - | RW | False |